(0)| 12/22/2022 4:54 PM | |
|
Joined: 5/6/2022 Last visit: 1/22/2026 Posts: 589 Rating:
|
Hi Mn6453shabad, As far as I can see, the migration of the project to version V7.3 SE you have started from version V6.2 and as far as I have checked, this migration must be done from V6.2 SP3. Have you done it from this version or as it says in the post you started from V6.2 without SP? Anyway, even if it is possible that you have already checked it, I recommend you have a look at the FAQ that I share with you where you can find information about the project migration from V6.2 to V7, if you still did it. At the end of the link, you will find a PDF document with more information. "How do you migrate WinCC projects to new versions of WinCC from V4 to V7?" I hope it will help you. Best regards! |
|
If this Information really helps, you could use the Rate function |
|
| 12/24/2022 4:53 PM | |
|
Joined: 12/20/2019 Last visit: 8/31/2025 Posts: 70 Rating:
|
|
Follow us on