(0)| 2/15/2023 9:21 AM | |
|
Joined: 5/1/2020 Last visit: 12/18/2025 Posts: 72 Rating:
|
Hello thank you for your response, I am using winCC V7.5 SP1 Upd 4 ( i erroneously assumed you would expect me to post on the correct forum haha) No virtual Machines are running both the client and server pcs are on their standard built-in OS. I have completely disabled the firewall on the server-pc given that it is not in the domain the client pc i cannot do the same given that the firewall rules are set by the domain administrator. The project has been migrated in the past from wincc v6.3 to 7.5 sp1 upd4 but that was 4 years ago with no issues. The current project is from a duplicate project using project duplicator with the save as function that i did as a backup like 3 months ago. The connection with one client for example is on the same switch and they share the same vlan so i would guess 1 hop. i run the cmd command tracert with the client ip and returned 1 1ms 1ms 1ms. There is no redundancy. I cannot start via interconnect because as i said client doesnt see server in simatic shell while server sees client as you will see in attached images. Attachmentclient simatic shell.zip (588 Downloads) |
| 2/16/2023 10:23 AM | |
|
Joined: 8/3/2009 Last visit: 1/22/2026 Posts: 16658 Rating:
|
Hello Gdim93 Check first the basics: Every station has to be set up with: https://support.industry.siemens.com/cs/de/en/view/868014 then check: https://support.industry.siemens.com/cs/de/en/view/109771695 If you cannot get it work to see each other in the Simatic Shell then try to set each other as Multicast Proxy and do a restart (its made for other usecases but should also help in your case) Bye Murof |
Last edited by: Murof at: 02/16/2023 10:30:29If this Information really helps, you could use the Rate function |
|
Follow us on