3/20/2019 11:20 PM | |
Joined: 9/19/2009 Last visit: 5/10/2025 Posts: 460 Rating:
|
Hi There is some tricks that you can use. I don´t know the order of the execution but if you can try this. Open Event execute VBScript code, and the last statement you can call the event of another push button , this button have your C code. Other way to do it is with Global Script and the trigger an internal tag, and one Script call another Script, don´t matter with is the languaje VBScript / ANSI C Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
This contribution was helpful to
1 thankful Users |
Follow us on