(0)| 8/30/2023 8:11 AM | |
|
Joined: 9/15/2022 Last visit: 1/16/2026 Posts: 18 Rating:
|
User Archive Control problem same problem in WinCC 7.2 SP2 I presume "Start value" would be the same, but it is not editable for Date fields! The problem is even more severe, if you ADD a field AFTER the user archive has been created and used. For example in a software upgrade, let's say the customer wants a date/time field added to the user archive. You add it, and then all the existing records have an empty value. The values of the following tags could not be written and you have to manually add an initial value to all existing records on the customer's user-archive. Regards, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/25/2023 10:05:22New subject after splitting Last edited by: MakisCE at: 09/25/2023 11:20:21 |
|
Follow us on