11/29/2023 7:16 PM | |
Joined: 11/28/2023 Last visit: 2/7/2025 Posts: 2 Rating:
|
Hello Gents, We have redundant system on HVAC AHU system , one of the PLC 412-5H PN/DP (FW v6.0.4; boot loader 6.00) has failed, replaced with new CPU with the same order 6ES7412-5HK06-0AB0 but FW 6.010 and boot loader 6.0.1. Uploaded backup project to the new PLC - doesn't go to RUN - came up with Error OB72 - system program different. Due to operation reasons could not stop HVAC so that Downgraded new PLC to FW v6.0.4. boot loader remains 6.0.1. Now we have Redundancy error OB72 - Link Up - update aborted due to configuration change Gents, Could you please advise ------------------------------------------------------------------------------------------ AttachmentDiagnose1.txt (515 Downloads) |
Last edited by: AutoGen_548893 at: 11/29/2023 19:38:34Last edited by: Jen_Moderator at: 11/30/2023 11:36:04New subject after splitting |
|
11/30/2023 11:39 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject Event ID 16# 73C1 is published within the conference SIMATIC S7-400 / S7-400H / S7-400F /FH. Jen_Moderator |
Follow us on