Default Header
(header konnte nicht geladen werden)
2/8/2024 5:39 AM | |
Joined: 7/31/2021 Last visit: 2/8/2024 Posts: 7 Rating: (0) |
Hello I am playing with the idea to control my electrical heating system . The heating system contains of two separate accumulation stoves ( unit with bricks heated by a resistor). I also have a lot of solar panels I have already installed a pulse signal for my energy consumation/production. A pulse signal for every Wh for import electricity and a pulse signal for every Wh for export electricity When in winter and the sun is shining , the stoves should be charging. But only with the power I produce. The energy company makes every 15 minutes a measurement of my enery consumation/production. How should I begin with this situation? First measure 10 minutes the enery production , and then 5 minutes or less consume the energy??? Dont' know where to begin Regards
AttachmentOude heibaan 35 versie 1.6.zip (192 Downloads) |
Follow us on