1/26/2024 11:36 AM | |
Joined: 2/17/2020 Last visit: 9/11/2025 Posts: 1251 Rating:
|
Hi, From WinCC V7.5 SP1, it is possible to establish a connection to a redundant S7- 1500 system. The procedure for this is described in the WinCC Information System: SIMATIC HMI WinCC V7.5 SP1 WinCC Information System > Communication > SIMATIC S7-1200, S7-1500 Channel > Channel configuration: WinCC V7.5 SP1 WinCC Information System > Redundant System S7-1500R/H |
A rating will be well appreciated. |
|
2/8/2024 12:37 PM | |
Joined: 3/30/2017 Last visit: 10/14/2024 Posts: 6 Rating:
|
Hi Murof Could you please explain how to switch the IP address of the accesspoint ? Thanks |
2/8/2024 1:10 PM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello I think it should be all explained in here: https://support.industry.siemens.com/cs/ww/en/view/109772961/127349029387?dl=en Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on