(0)| 4/17/2024 9:49 AM | |
|
Joined: 3/19/2019 Last visit: 5/28/2025 Posts: 26 Rating:
|
Dear Experts, Please help me slove my issue. Problem details. PLC was running ok without any error, suddenly today morning NODE - 5 ( SEW communication module for sew drive communication) fault occurred, after fault reset NODE fault reset and when i give command to sew drive it start and run for 10sec again node 5 fault was coming, in that SEW module total 7drives connected, out of 7 drives 5 was working ok after fault reset. When i give the command to 6 and 7 it just starts for few sec and again node fault was comming if i reset error goes and again comes during next start. I cheanged the SEW communication module also but still the problem is not resloved. I changed the profibus connecter and cable too. Please hlep me reslove this issue. Thanks VMK AttachmentDiagnose.txt (671 Downloads) |
Follow us on