5/5/2024 5:10 PM | |
Joined: 7/16/2021 Last visit: 5/8/2024 Posts: 7 Rating: (0) |
I have an RTD PT100 temperature probe, I want to read the temperature value displayed on the screen, through the AI pin of PLC LOGO, and read it with the AM2 RTD expansion module. Can someone please help me with an example? I'm new to PLC LOGO so I don't understand much about analog function blocks to use them properly. AttachmentPictures.zip (12 Downloads) |
Last edited by: Jen_Moderator at: 05/06/2024 09:47:28Text formatting optimized. Last edited by: Jen_Moderator at: 05/06/2024 09:48:32All pictures added as .zip file. |
|
5/5/2024 6:46 PM | |
Joined: 6/20/2010 Last visit: 5/26/2024 Posts: 87 Rating: (0) |
You also have to program the internal module of the probe (pt100 to 4-20 mA converter) with a specific program. |
Follow us on