Default Header
(header konnte nicht geladen werden)
(1)| 6/22/2009 8:41 PM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello, Perhaps in following FAQ you could find info: What can you do when the power requirement of the modules in the subrack exceeds the power supply provided by the CPU on the backplane bus? Regards Hristo Mihalev |
| 6/23/2009 1:39 PM | |
|
Posts: 76 Rating:
|
Hi, As it is written in ST70, each DI16 needs 25 mA and DO16 needs 80 mA. So, it seems 800 mA is enough! Good luck! |
Follow us on