Default Header
(header konnte nicht geladen werden)
(0)| 6/25/2009 6:40 PM | |
|
Joined: 7/2/2008 Last visit: 12/21/2025 Posts: 929 Rating:
|
Hello Lalit, The selection is through jumper and the rated input current is 2 A for 110VAC and 1 A for 220VAC Please download this manual. You will find all information you need there. Best regards. H-H |
| 6/25/2009 7:01 PM | |
|
Joined: 5/28/2008 Last visit: 1/14/2026 Posts: 4522 Rating:
|
Hello, The power supply input voltage is 120/ 230 VAC. It could be selected via a red selector switch in the front of the power supply. See the attached picture. If you have moved the selector upwords, it will be for 120VAC. Regards, |
Last edited by: Ayman Elotaify at: 6/25/2009 7:02 PMAyman Elotaify |
|
Follow us on