Default Header
(header konnte nicht geladen werden)
(1)| 6/25/2009 12:30 PM | |
|
Posts: 691 Rating:
|
Go through the attached procedure for connecting the tags in the block icons
AttachmentNew Folder.zip (350 Downloads) |
Last edited by: Niranjan at: 6/25/2009 12:36 PM |
|
| 6/25/2009 1:37 PM | |
|
Joined: 1/4/2008 Last visit: 12/22/2025 Posts: 703 Rating:
|
Hello anthuan, I thought it was solved already in this your thread. The solution of connecting the object to structured tag is still the same, in the pictures attached by Niranjan you'll see the wizard from the manual which you couldn't found in WinCC V6.2 because it's from the PCS7. The "interconnection" of the block icon with the faceplate is done by the C-script on mouse click, it should be already prepared on the block icon template. Which faceplate should be opened is determined from the object property Servername (before "Control"), normally in General part. The faceplate pictures also contains this standard object name in the picture name (normally after "@PG_"). Regards Sydney |
| 6/26/2009 8:21 AM | |
|
Posts: 54 Rating:
|
Yes, I see, thanks so much. anhtuan_ntc. |
Follow us on