(0)| 8/19/2024 4:29 AM | |
|
Joined: 4/28/2021 Last visit: 9/11/2025 Posts: 2 Rating:
|
It seems that the version I'm using is WinCC Runtime V7.5+SP2+Upd9 (K7.5.2.9). For a Static Text object: You can easily edit the text by double-clicking on it. For a Customized Object: If you right-click and go to "Customized Object" => "Create...", then select "UserDefined2" under "Selected Properties". With "Static Text" selected in "Objects", add "Text" by double-clicking under "Properties". Click "OK" to create the object, select the "UserDefined2" tab, and double-click on "Text". A "Text Input" box will appear, and you need to double-click "English (United States)" to modify the text. Summary: For a Static Text object: You can directly edit the text by double-clicking on it. For a Customized Object: When you double-click on "Text", a "Text Input" box appears, and you need to double-click "English (United States)" to modify the text. What I want to achieve: After creating a Customized Object and adding the "Text" feature, I want to make it so that I can edit the text directly without needing to go through additional steps. Note: This question was generated using a translation tool, so the sentences might be awkward. Note 2: How did you include multiple images? Attachment1234.zip (339 Downloads) |
Last edited by: SIM99 at: 08/19/2024 04:30:25Last edited by: SIM99 at: 08/19/2024 04:31:14 |
|
Follow us on