11/6/2024 10:52 AM | |
Joined: 2/4/2019 Last visit: 9/10/2025 Posts: 4 Rating:
|
Are there any updates? I have a similar issue, but this time with the CPU410-5H controller. It’s a brand new controller, and the problem is recurring. About a year ago, I had this issue and eventually had to load with the CPU stopped. Since then, I was able to make changes HW in RUN without stopping the CPU. Each time I made changes in RUN, some modules on the Profibus were missing—sometimes more, sometimes fewer—and it wasn't an issue. Now, the only difference is that fewer devices are inactive on Profibus DP—about 3 or 4 out of 70—and I can no longer load in RUN. Why? Nothing has changed compared to a month ago. Does anyone have any advice or useful documentation?
------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 11/06/2024 11:56:24New subject after splitting Last edited by: Moderator_Lan at: 11/06/2024 11:57:26Quote added |
|
11/6/2024 2:37 PM | |
Joined: 5/30/2022 Last visit: 9/10/2025 Posts: 634 Rating:
|
Hi, The following link details the options for downloading in RUN, I hope it is helpful, it also applies to SIMATIC MANAGER. Downloading blocks in the "RUN" operating mode to the device |
If this information really helps, you could use the Rate function. |
|
1/7/2025 7:28 AM | |
Joined: 7/16/2021 Last visit: 1/7/2025 Posts: 10 Rating:
|
|
Follow us on