(0)| 4/12/2019 4:15 PM | |
|
Joined: 4/15/2009 Last visit: 1/19/2026 Posts: 149 Rating:
|
Hello Jay, The 3RW44 softstarter has a thermal motor model and you set the prewarning motor heat build up 80%.Therefore you get a message when the thermal motor model has 80%. Perhaps reduce the switching frequency or set the prewarning limit of 80% to a higher value. Best regards Frank |
This contribution was helpful to
|
|
| 1/21/2025 7:46 AM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Joined: 1/21/2025 Last visit: 7/26/2025 Posts: 1 Rating:
|
Hello, we have installed a 3RW44 Soft Starter to start a air compressor. However, after only one or two hours working this drive sends me a warning "Prewarning limit motor built-up". Here follows the motor plate data:
There is no temperature sensor. The actual current on the motor is 179 Amp and it was showing the prewarning temperature message. As the motor currents are normal, i beleive, the softstarter shouldn't have a prewarning messages. Anyone has an idea? Thanks Rakesh |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Follow us on