Default Header
(header konnte nicht geladen werden)
(0)| 2/20/2025 9:49 AM | |
|
Joined: 8/14/2024 Last visit: 7/29/2025 Posts: 20 Rating:
|
Hi everyone, I need assistance in connecting the CPU 1513R-1 PN with ET200SP in R1 redundancy. Since there weren't enough reference manuals available, I connected the modules based on the existing Siemens documentation (see attachment). I have also included the TIA Selection file. Could you please check if the attached architecture is correct? If not, where can I find the appropriate reference manuals? Thank you!
AttachmentCPU-1513-1 PN_with_ ET200SP R1 architecture.zip (206 Downloads) |
Follow us on