(0)| 3/3/2025 3:08 PM | |
|
Joined: 1/12/2023 Last visit: 12/28/2025 Posts: 1 Rating:
|
Hello to everyone. Aslo I got new verison of Jumo LOGOSCREEN700 and like to set communication over Modbus with LOGO! Have LOGO!: 6ED1 052-1MD08-0BA1, LogoSoft V8.3. I was able to get temperature value of AI1 from Jumo via Modbus on LOGO!, ... but can't send digital value (M1) from LOGO! to Jumo and record that value state. On online test read bit M1=V1104.0, M2= V1104.1, but not see on Jumo700. Also try mapping with V100.0 an V100.1 Try different datatype, addresses ... not sure that i missing... if anyone have some solution i appriciatet ------------------------------------------------------------------------------------------ Attachmenttest 1.zip (224 Downloads) |
Last edited by: Moderator_Lan at: 03/03/2025 15:11:09New subject after splitting |
|
| 3/3/2025 4:58 PM | |
|
Joined: 12/18/2014 Last visit: 1/14/2026 Posts: 36451 Rating:
|
If I were you, I would make the LOGO! as the client and the JUMO as the server. |
Follow us on