Default Header
(header konnte nicht geladen werden)
7/27/2009 1:37 PM | |
Joined: 5/8/2006 Last visit: 10/16/2024 Posts: 1085 Rating:
|
Hi The only difference between the OP27 mono and OP27 color ist the display. If you use the same HMI project with the same ProTool version, thenit should works. You wrote that the OP27 hang sometimes during the process.Do you modify something on the hardware? Bye |
Follow us on