Default Header
(header konnte nicht geladen werden)
(2)| 7/14/2006 12:19 PM | |
|
Posts: 1084 Rating:
|
Hi, Please note that the time of the SQL Server is in UTC time, and could therfore be different then the local time set on your pc ! with regards, Ikkezelf |
| 7/14/2006 12:48 PM | |
|
Posts: 54 Rating:
|
Yes you are right. I didn't cathc that because I've used statical data. Many thanks. |
| 7/20/2006 6:16 PM | |
|
Posts: 54 Rating:
|
Any idea why I didn't succeded connecting with CC_ExternalBrowsing ? |
| 7/21/2006 9:18 AM | |
|
Posts: 1398 Rating:
|
Open Start -> Programs -> Microsoft SQL Server -> Enterprise Manager. Expand the tree to see your server and the databases in it. Can you see a CC_ExternalBrowsing database ? |
| 7/21/2006 10:45 AM | |
|
Posts: 54 Rating:
|
Salma, no there is no CC_ExternalBrowsing database. |
| 7/21/2006 10:49 AM | |
|
Posts: 1398 Rating:
|
That would explain why it does not work [:D] You only get this database when you install the Connectivity Pack Server. You could try installing (or reinstalling if it is already there). |
| 7/21/2006 10:56 AM | |
|
Posts: 54 Rating:
|
Yes it does. I've installed the connectivity pack client. As I've read in the help it is enough for reading the databases. Is the price different for client / server ? 10x once again |
| 7/21/2006 11:02 AM | |
|
Posts: 1398 Rating:
|
Hi It is the same license for the server and the clients [:D] You install the Connectivity Pack Server and the license on the WinCC machine. You can then install the Connectivity Pack client on any remote computers that need it. You do not need to install a Connectivity Pack license on these remote computers. Salma |
| 7/21/2006 11:49 AM | |
|
Posts: 54 Rating:
|
Oh I've missed that. Thank you |
Follow us on