Default Header
(header konnte nicht geladen werden)
(0)| 10/14/2009 3:29 PM | |
|
Posts: 18 Rating:
|
Dear All, While adding a new software logic to my CPU, after finishing compiling succesfully, during attempt of download, I have received the alarm of "Low Work Memory after download". You can see the warning message at the attached picture. I cancelled the download and checked the CPU Module information, available workin memory is 86%. System is suggesting to compress but i think it will need CPU stoppage which is not possible at the moment. Question is, if i download the software changes, what may happen? Thanks in advance... Canan Tas AttachmentSM.zip (435 Downloads) |
Follow us on