Default Header
(header konnte nicht geladen werden)
(0)| 12/22/2009 1:37 AM | |
|
Posts: 25 Rating:
|
Dear everyone, IF you know this, please help me. Thanks so much. Best regard leegiang |
| 12/22/2009 9:49 AM | |
|
Joined: 12/9/2009 Last visit: 10/30/2025 Posts: 156 Rating:
|
Hello, Do I understand right??? You want to exchange data between CPU315-2DP and Fuzzy control via PROFIBUS? There are any other components in you S7-300 station? The CPU 315-2DP supports for example DP protocol. That means you can configure the CPU as DP master or DP slave in STEP 7. If Fuzzy control supports DP slave or DP master it should be possible to exchange data between the systems. In this case the CPU 315-2DP works for example as DP master and Fuzzy control as DP slave or the other way around. Here are some articles about configuration of S7-300 station: http://support.automation.siemens.com/WW/view/en/13091565 http://support.automation.siemens.com/WW/view/en/7764609 Good Luck |
This contribution was helpful to
|
|
| 2/14/2010 10:23 PM | |
|
Joined: 10/3/2008 Last visit: 1/14/2026 Posts: 996 Rating:
|
Hi, did you solve your problem? Wüstenräuber |
Follow us on