Default Header
(header konnte nicht geladen werden)
7/9/2010 8:10 PM | |
Posts: 13 Rating: (0) |
Hello dear LOGO! experts , I have encountered with three problems and i hope that you can help me to solve them. [schnippschnapp] 2. I need to see and register the start time & date of my project(a project may last five days) on the LOGO screen, i have done such a thing by using message enable time & date but the problem is that sometimes i need to turn-off the machine & LOGO together in the middle of the project(e.g. in the end of work time) so when i restart the machine & LOGO the new start time & date overwrites. and i can't see the old start time witch is the start time of my project, it's clear that message enable time & date is not retentive so do you know any other way to register start time & date despite the LOGO being turned off ?
[schnippschnapp] Other two questions are splitted into the following threads i want to monitor and archive the status of digital . Cycle time delay. |
Last edited by: O_Moderator at: 7/12/2010 12:10 PMnew subject after splitting |
|
Follow us on