Default Header
(header konnte nicht geladen werden)
(0)| 9/27/2010 11:26 AM | |
|
Joined: 7/2/2008 Last visit: 12/21/2025 Posts: 929 Rating:
|
Hello EFJ, To the best of my knowledge, the CIR (Configuration In Run) is restricted to the use of Profibus masterwith S7-400. You can read more about CIR in: Modifying the System during Operation via CiR Which slaves can be added as modular slaves with CiR to a DP master system and which system requirements are necessary in the master system? Best regards. H-H |
Follow us on