Default Header
(header konnte nicht geladen werden)
(0)| 10/25/2010 5:54 PM | |
|
Joined: 7/2/2008 Last visit: 12/21/2025 Posts: 929 Rating:
|
Hello stoprak, I hope you find the following links useful. S7-400H+CP443-1 with Kepware How do you configure a fault-tolerant S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software? How do you configure a fault-tolerant S7 connection for the SIMATIC NET OPC server via Industrial Ethernet with the SIMATIC NET PC software? Best regards. H-H |
| 10/26/2010 11:55 AM | |
|
Joined: 7/2/2008 Last visit: 12/21/2025 Posts: 929 Rating:
|
Hello stoprak, Tothe best of my knowledge, you must go for SIMATIC Net OPC if you are going to use RED. CONNECT. I checked the KEPserver EX OPC and found that it doesn't have the required driver for redundant connection with S7-400H. Bets regards. H-H |
Follow us on