Default Header
(header konnte nicht geladen werden)
(1)| 10/15/2010 4:52 PM | |
|
Posts: 24 Rating:
|
Hi All H systems have capabilities of F block processing but they just process standard programs. This is my question: "How to distinguish pure H and HF CPUs" Splitted from F CPUs properties. |
Last edited by: O_Moderator at: 10/18/2010 9:31 AMnew subject after splitting |
|
| 10/26/2010 11:27 AM | |
|
Joined: 7/2/2008 Last visit: 12/21/2025 Posts: 929 Rating:
|
Hello ELSAVAN,
Visually, the F-CPU should have a yellow TUV stickers. You should also see some distributed fail safe I/O modules connectedCPUs. They will also have yellow labels. And youmay alsosee TUV logo printed on the module itself (Only wide modules - 8cm) From a software point of view, If you try to upload, it must ask you for a password. If you have hardware configuration with you then you will see, 1- In CPU properties, H parameters tab, you will see a number for OB with special handling (normally OB35). If it's just an H-system then you will see 0 instead of 35. 2- In CPU properties, protection tab, you will see the check mark for CPU contains safety program. Best regards. H-H |
This contribution was helpful to
|
|
| 10/31/2010 7:44 PM | |
|
Posts: 24 Rating:
|
Thanks H-H , it is very helpful Elsavan |
This contribution was helpful to
|
|
Follow us on