Default Header
(header konnte nicht geladen werden)
(0)| 11/11/2010 12:24 AM | |
|
Joined: 7/2/2008 Last visit: 12/21/2025 Posts: 929 Rating:
|
Hello egy_eng, The new CPU is quite bigger in terms of memory and addressable area. It's also quite faster and you will be happy comparing the scan cycle of both CPUs. You can compare between both using the following links. 6ES7416-2XK02-0AB0 6ES7416-2XN05-0AB0 All you have to do is to right click on the old CPU in hardware configuration and go to replace object and select the new CPU and everything should work fine. You don't need to edit anything in the software. Best regards. H-H |
| 11/11/2010 8:01 AM | |
|
Posts: 43 Rating:
|
Dear H-H , thank you very much for your help and it is very appreciated. regards |
Follow us on