Default Header
(header konnte nicht geladen werden)
11/11/2010 5:14 PM | |
Joined: 6/24/2010 Last visit: 12/7/2021 Posts: 21 Rating:
|
Hi All, I'm wondering if anyone has recently had any experiance with dimming light circuits via a logo. I am looking to implement a soft start function as well as security/mood lighting (100%/ 30-50%) output. I was wondering about using a trans output unit driving solid state relays with a PWM signal but not sure if this would cause flickering?! I have seen this post: /tf/WW/en/Posts/4628 but the links are no longer valid.The 0-10v dimmers i have found all seem to be for fluorescent lamps or HID'sbut i need them tobe used for incandesant and 240v halogen lamps. Any advise would be greatly appreicated. Rich |
11/19/2010 12:31 AM | |
Joined: 6/24/2010 Last visit: 12/7/2021 Posts: 21 Rating:
|
Has nobody tried this before? |
11/19/2010 2:37 PM | |
Joined: 10/15/2010 Last visit: 3/1/2023 Posts: 6 Rating:
|
I would look at something like this: 0-10V interface. This is designed for Halogen lighting. I'm sure there similar interfaces for incandecent light. Osram site SS Relay may be too slow.if you take 50% of the sinewave starting at the zero crossing, you would have to be on for 4 ms for every 8 ms. Waffleman |
11/19/2010 6:28 PM | |
Joined: 6/24/2010 Last visit: 12/7/2021 Posts: 21 Rating:
|
Got it. Many thanks for that. Rich |
Follow us on