8/17/2011 4:21 AM | |
Joined: 10/7/2005 Last visit: 9/3/2025 Posts: 3049 Rating:
|
Hello Begginer it depends would be my answer in this case. you can generally use an IM463-2 <-> IM314 combination to use S5 I/O's with an S7-400 (see HERE for more). You can also do so with an S7-400 H CPU, but must in this case operate it in so called "stand-alone mode" which is possibly NOT what you want to do (see AppendixB of the SIMATIC Fault-tolerant Systems S7-400Hfor more on this). I hope this helps |
Cheers |
|
8/17/2011 4:21 PM | |
Posts: 112 Rating:
|
Hi Fritz, My CPU will be redundant s7-412H, is this capable to use the old non redundant s5-IO but have two 6ES5324-3UR11? Thank you in advance |
Follow us on