Default Header
(header konnte nicht geladen werden)
(0)| 8/8/2012 7:21 AM | |
|
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, First, that's a verry old logo, so not mutch functions are in it. You can program it with the keys on the logo itself or with Logosoft. How you can read in the manual There are 2 types of cables: RS232 and USB I The logo type you have can not be expanded, so all you need is a powersupply. Compatibility overview of LOGO! Basic and LOGO! Expansion modules. If you program with Logosoft first select your type of Logo(select hardware ctrl+H), otherwise you can build a program that doesn't fit in you type of logo. Regards, Marcjan |
Last edited by: Marcjan at: 8/8/2012 7:28 AMLast edited by: Marcjan at: 8/8/2012 7:24 AMProblem solved? |
|
Follow us on