Default Header
(header konnte nicht geladen werden)
(0)| 2/20/2013 12:15 PM | |
|
Posts: 179 Rating:
|
thank you very much mike for answer first of all 1-client request us to use siprotec device and BCU from siemens because he want to extend his substation . 2-the exsit vendor is ingteam company using PROCOME protocol between UCS(substaion control unite) it is collect data from BCU(TCP-m) and protection devices and then dend it to Control center and HMI . 3-i must give him an answer with yes we can connect siemens device support this type of protocol or not ? 4-i have read in the manul Ingteam product that if you need to connect device support IEC61850 you should contact us. what should i do? thank you very much to support me Attachment15PG-00-BBY-EMP-IGT-004 Rev 0 - UCS_IH_Info.pdf (419 Downloads) |
Follow us on