Default Header
(header konnte nicht geladen werden)
(0)| 3/31/2013 2:05 PM | |
|
Joined: 8/31/2010 Last visit: 12/6/2025 Posts: 1525 Rating:
|
Hello amsd, You can connect a maximum of 8. But it is better to know the limitations of S7-1200 communication with WinCC Flexible RunTime as mentioned in this. - How do you access S7-1200 tags with a panel or RT configured with WinCC flexible 2008 SP2? If you want to have a seamless communication then WinCC Advanced v12 should do. You can connect on Ethernet. |
|
Like it? Rate it! |
|
Follow us on