Default Header
(header konnte nicht geladen werden)
(0)| 6/18/2013 5:45 PM | |
|
Posts: 767 Rating:
|
Hello Rich42, Per attachment from SIMODRIVE 611 universal Description of Functionsif part number of power module isnot a zero in last digit(it could be a0, 1, 2,or 3 currently) then the control unit has automaticpower module identification which loads power module code in P1106. An automatic power module identifcation routine is executed each time the control board runs-up. In this case, the value in P1106 is compared with the value of the power module identified in P1110. If the values are not the same, there is an error condition and an appropriate fault message is signaled. Deputy Attachment611 universal pm.pdf (575 Downloads) |
Last edited by: O_Moderator at: 6/18/2013 8:07 PM |
|
| 6/20/2013 8:57 PM | |
|
Posts: 2964 Rating:
|
Hello, Check this link.......i think you are getting the error 39 in your 611U drive /tf/WW/en/Posts/72721 Regards, Prakash |
Follow us on