10/2/2013 12:20 PM | |
Joined: 9/23/2005 Last visit: 9/3/2025 Posts: 4416 Rating:
|
Hi, one of the innovations of the SP1 for STEP7 V12 (Released for Delivery at http://support.automation.siemens.com/WW/view/de/76276623) is the inclusion of new instructions, like GetAlarmInfo for S7-1500. With this instruction it is possible know if an alarm is active/acknowledged in S7-1500. Here there is a very simple sample project to illustrate how it works. It has a very simple S7-1500 program and a HMI for data monitoring AttachmentC:\Users\z0008iwv\Documents\Bluetooth Exchange Folder\GetAlarmInfo.zip (1211 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to
1 thankful Users |
Follow us on