Default Header
(header konnte nicht geladen werden)
(0)| 3/11/2014 4:00 PM | |
|
Posts: 13 Rating:
|
Steven81: i can't adjust it. I'll have to deal with the 10 V DC motor ! huggy_d1: that's what i wanted to do in the last resort. But i found out another solution.. I'm using a TP temporisation with a value that matches my issue and it works great. The holes are at equal distance from eachother so basicly, all i've got to do is knowing the time needed to go from A to B or B to C. Once i know the time "T", set it as PT in the TP temporisation and the positionning of the object will be perfect ! Thanks for your replies !
|
This contribution was helpful to
|
|
Follow us on