Default Header
(header konnte nicht geladen werden)
(0)| 9/24/2007 6:46 PM | |
|
Posts: 68 Rating:
|
Hello, I can't launch a WinCC 5.1 SP1 project. When I try to do it, first the "Activating...." message appears. After several seconds the "Desactivating ..." message appears while launching the text library service, and the projectgoes to stop. I've seen in the \diagnose folder, exactly in the"WinCC_SStart_01.log" file that I attach, a problem when launching the Data Manager RunTime. Thank a lot ! AttachmentDiagnose.zip (181 Downloads) |
| 9/26/2007 9:34 AM | |
|
Posts: 68 Rating:
|
Good idea, But... even if I create anew emptyproject I obtain the same results. Thanks !. |
| 9/26/2007 10:17 AM | |
|
Posts: 170 Rating:
|
hi, do use step7 v5.2 on the same computer??? In this case you need a hotfix for wincc! http://support.automation.siemens.com/WW/view/de/14685938 |
| 9/26/2007 5:32 PM | |
|
Posts: 68 Rating:
|
Applies this to WinCC 5.1 SP1 version ? |
| 9/27/2007 8:34 AM | |
|
Posts: 1776 Rating:
|
Hi, Which softwarehave You installed on this computer? Maybe the installed software is not compatible. See http://support.automation.siemens.com/WW/view/en/21927668 April |
Follow us on