Default Header
(header konnte nicht geladen werden)
9/2/2014 7:57 AM | |
Posts: 5225 Rating:
|
Hi there. How ddo you implement your recipe? What type of motion controller are you using.. perhaps the internal motion control? I have a feeling that your issue is in the implementation of your concept. If you are not doing so already, please consider using the PLC's built-in motion control blocks. If it is practicle for your application is an open question. I have a positive feeling that the motion control' s Command Table will be helpful to you. I recommend for you to have a look at the CE-X7 example..[LINK] With more information (the more visual.. the better) the guys can be more helpful. Greetings. w |
Follow us on