Default Header
(header konnte nicht geladen werden)
(0)| 10/2/2014 3:33 PM | |
|
Posts: 158 Rating:
|
I'm not sure I could get it in backwards, but ok....when it's working properly, is it spring loaded? - do you push in to release it and get it out? |
| 10/2/2014 4:43 PM | |
|
Posts: 158 Rating:
|
oh boy. I did 2 trial data logs. I did not touch the program, and performed basically the same test, one before and one after removing the card slot from the PLC. The 1st run is an expected array of on/off data. The run after replacing the sd card gave me not only strange numbers, but truncated half of the inputs and all the outputs that should have been written. See attached. I think SIemens needs to revisit their manufacturing process on this plastic assembly...
Attachment2nd DL-tricked up lookin.pdf (355 Downloads) |
Follow us on