Default Header
(header konnte nicht geladen werden)
(0)| 10/25/2007 5:38 PM | |
|
Posts: 6 Rating:
|
Hi It's a Siemens panel PC 670 OS Win 2000 pro SP2 WinCC 5.1 no SP error upon restart of PC and WinCC 1. CCTlgserver.exe has generated errors and will be closed byWindows. You will need to restart the program. And the autostart function freezes. 3 number of h result errors When opening WinCC Explorer I get : 0x80004005 Unspecified error, then I click OK and get 0x2 The system can not find the file specified, next OK 0x80046204 : (null) OK Die Projektdaten konnten nicht gelesen werden, click OK (Project database could not be read) no more errors When I try a new project I don't get any errors but the editors in Explorer only go as far as Server Connections and structured taggs. Simatic software is AutorsW, simatic net cd 05 2000 sp2 build 2309, simatic hmi touch input (touch panel pc670), in WinCCstorage is installed but it seems not used. Also the first reason I began checking the panel is that the neither trend or alarm windows have any connection to their databases. I might try deinstall wincc 5.1 and install wincc 5.1 sp2 before I try reinstalling the whole PC. But it would be nice to know what theese errors are meening, I know what they meen in WinCC v6 but not in v5. Thanks Zeb Attachmentdiagnose.zip (152 Downloads) |
| 10/26/2007 12:39 PM | |
|
Posts: 1275 Rating:
|
Hi, About the 0x80046204 error, check this FAQ out. It's for v5 only! In your diagnose I found many entries like this: 255,25.10.2007,16:40:27:133,1003051,2,Administrator,CT-KRAFT,Alarm Logging RT,Quittiervaribale(Bit) schon von Einzelmeldung belegt But I don't speak german at all, so I have absolutely no idea what that means... I've also found 255,23.10.2007,09:32:44:045,0,4,Administrator,CT-KRAFT,CCDmTagProviderMux,Provider : CCDmTagLocal throws Exception in Method : ICCDmAsoEnum::GetCount() and 255,25.10.2007,16:40:46:671,0,4,Administrator,CT-KRAFT,CCDmTagProviderMux,Provider : CCDmTagLocal throws Exception in Method : ICCDmAsoEnum::EnumData() But I couldn't find anything on those.. Best regards, Danielle |
| 10/29/2007 11:58 AM | |
|
Posts: 1275 Rating:
|
Hi Zeb, Service packs do come to fix bugs... Best regards, Danielle |
Follow us on