Default Header
(header konnte nicht geladen werden)
(0)| 10/21/2014 11:21 AM | |
|
Posts: 2347 Rating:
|
Do you have a connection between the negative terminal of the battery and the M terminal of the LOGO !? According to the data sheet of MCP9700A are between a temperature of -40 ° C and +125 ° C from a voltage of 2.3 V to 3.95 V. Example, see attached file. AttachmentExample TS01.zip (262 Downloads) |
| 10/22/2014 4:11 PM | |
|
Posts: 2 Rating:
|
Thanks!It´s working now!. |
This contribution was helpful to
|
|
Follow us on