Default Header
(header konnte nicht geladen werden)
(0)| 10/27/2014 8:50 AM | |
|
Posts: 5 Rating:
|
hi hello , im facing the problem with Simocode motors which is configured with PCS-7 (s7-400 PLC) suddenly all the simocode motors stopped due to communication problem the alarm displayed in the System as general fault:(no1002) bus/ PLC due to this problem motor stopping and again starting in the auto conditions and the above mentioned alarm is displaying. give me the solution as soon as possible.
----------------------------------- New subject after splitting from SIMOCODE ES enter a number in trip level of Current limits. |
Last edited by: Min_Moderator at: 10/27/2014 2:26 PMsplitted |
|
Follow us on