(0)| 11/21/2007 10:45 AM | |
|
Posts: 4 Rating:
|
We have such a problem: There is a VB script in the project for archive tag database query through ADO DB, In my script (on button click) there are 6 queries (for 6 archive tags) in comparison with the example above, where Mostly the script is running well but sometimes the VB script engine hangs. If I deactivate the project then pdlrt.exe continues to hang in task manager processes. The script hangs in the following lines (I checked it with the help of HMIRuntime.Trace): In demo-projects (with the only archive tag request) several quick requests in a row contribute to the same What can I do? Connectivity pack is not installed. Do I really need it as the project can surely work without it...? By the way, is it possible to upgrade winCC sql server with service packs from the Microsoft web site? Attachmentscript.zip (208 Downloads) |
Last edited by: ilya_v at: 21.11.2007 10:47script.zip - is a txt file |
|
Follow us on