(1)| 11/23/2007 5:14 PM | |
|
Posts: 341 Rating:
|
Dear Forum, Is it possible to write 360 samples/second through OPC link into wincc database. I am using WinCC V6.2 SP2 , SQL 2005. Regards, rit03 |
| 11/27/2007 3:28 PM | |
|
Posts: 1398 Rating:
|
The question is do you want the data in the WinCC Tag Logging database or just the WinCC SQL Server. If it's the latter then it's easy, if it's the former then it's tricky and maybe not possible. There was mention a while ago that the WinCC OLEDB Provider would have the ability to write as well as read to the database (hence the TAG:R for read currently). I don't know if this is available yet but may be worth chasing up. Another option is to use the ODK function to insert data into the Tag Logging database. Not ideal and would require an intermediate loading area and a lot of scripting. Finally if the controller is an S7 then you can send the data from the PLC to WinCC. See this thread for more info: WinCC V6, fast archiving Hope this helps, Salma |
Follow us on