(0)| 11/28/2007 9:33 AM | |
|
Joined: 9/23/2005 Last visit: 1/16/2026 Posts: 80 Rating:
|
Hi, see this FAQ http://support.automation.siemens.com/WW/view/en/996777 http://support.automation.siemens.com/WW/view/en/21914125 Hope this help you. |
|
__________________________________________ |
|
| 11/29/2007 10:05 AM | |
|
Posts: 4 Rating:
|
http://www.automation-drives.ru/as/download/ascat/simatic_pcs7/readmev6.zip How to incorporate the Russian language into PCS7 v6.x 1st step. Settings in Win2000 1.1 ATTENTION I recommend to use the English version of Win2000, because, some German char is incompatible with Russian char. You don't need any additional software packages for Russian language, like a Cyrilika package. In Control Panel/Regional Settings you have to select the country Russian. Open the option "Set as default" and set Russian too.1.2 Open regedit and path HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Control\Nls\CodePage Set for code page 1250, 1251 and 1252 the same value 1251.nls2nd step. Incorporate the Russian language in to the PCS7 libraries. 2.1 Open needful library (PCS7 Library or BATCH library) in SIMATIC Manager and add the Russian language via Option/Display language.... 4th step. Changes in WinCC 4.1 IMPORTANT The code of Russian language in WinCC – 419(hex)/1049(Dec) Open WinCC/Text Library and add Russian language .... |
Follow us on