Default Header
(header konnte nicht geladen werden)
(0)| 12/10/2007 4:05 AM | |
|
Posts: 5 Rating:
|
Hi, all I came across a problem in my project that customers need a seperately acknowledgement function for different kind of messages in thefaceplate. For example, in valve faceplate, they have five kinds of messages: Alarm High, Alarm Low, Warning High, Warning Low and Fault. Therefore, five seperate buttons are neededtoacknowledge corresponding messages, one for Alarm High, one for Alarm Low.....ect. According to my idea, I am planning to create an addtional comment in Text 10 for each message in alarm logging. For instance, object "CA21V200" is a valve. A comment "CA21V200.AH" will be added in Text 10 for the alarm high message of this object. Then, I create a c scripton the mouse action of the acknowledge button, using the structure "MSG_RTCREATE_STRUCT" and function "MSRTCreateMsg". In which, I am planning to usecontent of Text10 as keyword to get the exact message and acknowledge it. But, actually, failed. The function can not be compiled successfully. PS: I noticed that there is limited information about structure "MSRTCreateMsg". Does anybody know where to get detail description of this structure? PS again AttachmentMsgAck.zip (191 Downloads) |
Last edited by: AlecksWang at: 10.12.2007 11:16 |
|
| 12/11/2007 11:44 AM | |
|
Posts: 1776 Rating:
|
Hi, can you use the FAQ http://support.automation.siemens.com/WW/view/de/25012006 see the limitation (remarks) at the end of the FAQ. Use the new function described in the FAQ. Hope you get success. April |
Follow us on