Default Header
(header konnte nicht geladen werden)
4/25/2008 3:00 AM | |
Posts: 191 Rating: (58) |
Hi!! if you are using the analog threshold trigger, then it is not possible directly, because this function does not allow to use the Reference of another function as a limit.. but you can use a trick and some SR blocks please look at the attachment Hope this helps!! ROSA Attachmenttemp.zip (668 Downloads) |
4/28/2008 6:15 PM | |
Posts: 191 Rating: (58) |
Ok!! then try this, and please post if it works.. ROSA Attachmenttemp.zip (720 Downloads) |
4/28/2008 8:52 PM | |
Joined: 4/24/2008 Last visit: 5/23/2024 Posts: 6 Rating: (0) |
Hi! You have forgoten that we only want to change 4 parameters! I think I have done the solution for refrigeration and for heating and if you don't mind you can see if it is correct. Kind regards, Luis AttachmentLogo.zip (632 Downloads) |
4/28/2008 9:56 PM | |
Posts: 191 Rating: (58) |
Hi!! it seems that your solution does what you need.. i hope the programs i sent could help you!! ROSA |
Follow us on