(0)| 3/2/2017 3:10 PM | |
|
Posts: 4 Rating:
|
Hi, good information here, but I am still having difficulty in setting up a functional Modbus Client/Server network. Configured the devices and IPs but I cannot add a circuit to any device. Conversely if I create a separate (new) circuit using a Network Input or Output block I get an "incompatible connector" error when I try to add any input conditioning for the block. What am I doing wrong? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/2/2017 4:51:02 PMNew subject after splitting |
|
| 3/2/2017 3:20 PM | |
|
Joined: 12/18/2014 Last visit: 1/19/2026 Posts: 36483 Rating:
|
Please upload your LOGO! Program to the Forum. |
| 3/2/2017 4:34 PM | |
|
Posts: 4 Rating:
|
Here you go. Not much there. Basically trying to create a Modbus test network with LOGO (client) and AB Micro 820 (server). Thanks AttachmentDW_LOGO_Micro820Test.zip (435 Downloads) |
| 3/2/2017 5:22 PM | |
|
Joined: 12/18/2014 Last visit: 1/19/2026 Posts: 36483 Rating:
|
In the Network view, select only 2 MODBUS compatible devices. However, you must select at least one LOGO! 8.FS04 instead. And with the IP addresses it will not work. The LOGO! has network class 3, since the IP address must begin with 192.xxx.xxx.xxx. AttachmentDW_LOGO_Micro820Test_V2.zip (440 Downloads) |
This contribution was helpful to
|
|
| 3/2/2017 6:05 PM | |
|
Joined: 12/18/2014 Last visit: 1/19/2026 Posts: 36483 Rating:
|
In the attached video, you can see how make the connection between LOGO! (client) and MODBUS device (server).
AttachmentTest.wmv (662 Downloads) |
Follow us on