Default Header
(header konnte nicht geladen werden)
(0)| 5/14/2008 6:42 AM | |
|
Posts: 56 Rating:
|
Dear sir I have MP370 Operating panel.I want to down load the project file into it.Please tell me which Cable is required and Procedure to down load |
| 5/14/2008 7:43 AM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello tt_singh; Is this a Prosave bacup, or a Protool/WinCC flexible project file? For Prosave restore, look at the following FAQ. In any case, the FAQ discusses the different cables you can use to connect to the panel, using different interfaces (this is valid for a project download also): http://support.automation.siemens.com/WW/view/en/28928853 The ProTool/WinCC Flexible download procedure is discussed in the MP370 manual; I have prepared an extract that gives you barebones instructions. Hope this helps, Daniel Chartier AttachmentMP370_download.zip (533 Downloads) |
| 5/15/2008 5:40 PM | |
|
Posts: 993 Rating:
|
Hi, maybe this FAQ will help you: http://support.automation.siemens.com/WW/view/de/19109408 Bye |
Follow us on