Default Header
(header konnte nicht geladen werden)
(0)| 7/5/2008 6:50 AM | |
|
Posts: 3 Rating:
|
I'm learn in WinCC,I creat 2 files : "van_name.pdl" and "van_control.pdl". I want to do following : when I active them: 1. When I Click mouse on Van_name.pld ( Click on "4" in Object name), Picture name "van_control.pld" will appear and only appear object name (" 5" in attach file). and "5" will appear above "4" one distance following "6". Best regards! Attachmentexample.zip (86 Downloads) |
Follow us on