Default Header
(header konnte nicht geladen werden)
(0)| 7/17/2008 11:03 AM | |
|
Posts: 10 Rating:
|
My custumers want to use PC to controlHMI using Ethernet, Please help me chose the type HMI and how to configure HMI and PC. |
| 7/17/2008 11:45 AM | |
|
Joined: 4/24/2006 Last visit: 1/20/2026 Posts: 9106 Rating:
|
Dear HNLinh, Please have a look at following links: http://support.automation.siemens.com/WW/view/en/26331265 http://support.automation.siemens.com/WW/view/en/19865167 Perhaps they are useful. Best regards, Wizard |
| 7/17/2008 11:53 AM | |
|
Posts: 14 Rating:
|
Hello There are some options (software)to do that you want. What kind of PLC are you using (S7-200, 300, 400)? In order to do your application you can use: WinCC Flexible (RT) WinCC flexible Getting Started http://support.automation.siemens.com/WW/view/en/18660846 WinCC flexible 2007 Runtime http://support.automation.siemens.com/WW/view/en/18795593 WinCC flexible Getting Started Advanced http://support.automation.siemens.com/WW/view/en/18656980 WinCC WinCC V7.0 Getting started http://support.automation.siemens.com/WW/view/en/29221062 Please check these information from the links and select the better option. In both cases you can use your ethernet interface for the communicaction. Best regards. |
Follow us on