Default Header
(header konnte nicht geladen werden)
(0)| 8/4/2008 6:05 AM | |
|
Posts: 12 Rating:
|
Can I use a standard SD memory card in OP277 panel? |
| 8/4/2008 10:18 AM | |
|
Posts: 1611 Rating:
|
Hi, i mean (and ido it) you can use standard CF Cards. In some cases it could be, that the cards does not works, so the best are you buy a memory card and test it (when its works, then you can buy more!) Notes: Siemens give only of his cards a guarantee for work! Furthermore: Notes the different between CE3.0 and CE5.0 panels. (memory of the cards) -> http://support.automation.siemens.com/WW/view/en/21847868 regards, |
Follow us on